Cart  |  Contact  |  Help  |  auinfo@dwyeromega.com  | 
Toll-Free in Australia: 1800 106 210
International+65 6415 5353

Accelerometers

Introduction to Acceleration Measurement

An accelerometer is a device that measures the vibration, or acceleration of motion of a structure. The force caused by vibration or a change in motion (acceleration) causes the mass to "squeeze" the piezoelectric material which produces an electrical charge that is proportional to the force exerted upon it. Since the charge is proportional to the force, and the mass is a constant, then the charge is also proportional to the acceleration.

OMEGA Engineering offers a wide range of accelerometers in Australia.

Accelerometers

Learn more about accelerometers

piezoelectric force sensor

A piezoelectric force sensor is almost as rigid as a comparably proportioned piece of solid steel. This stiffness and strength allows these sensors to be directly inserted into machines as part of their structure.

Accelerometers Types

There are two types of piezoelectric accelerometers (vibration sensors). The first type is a "high impedance" charge output accelerometer. In this type of accelerometer the piezoelectric crystal produces an electrical charge which is connected directly to the measurement instruments. The charge output requires special accommodations and instrumentation most commonly found in research facilities. This type of accelerometer is also used in high temperature applications (>120C) where low impedance models can not be used.

The second type of accelerometer is a low impedance output accelerometer. A low impedance accelerometer has a charge accelerometer as its front end but has a tiny built-in micro-circuit and FET transistor that converts that charge into a low impedance voltage that can easily interface with standard instrumentation. This type of accelerometer is commonly used in industry. An accelerometer power supply like the ACC-PS1, provides the proper power to the microcircuit 18 to 24 V @ 2 mA constant current and removes the DC bias level, they typically produces a zero based output signal up to +/- 5V depending upon the mV/g rating of the accelerometer. All OMEGA(R) accelerometers are this low impedance type.

Accelerometer Specifications


Dynamic Range is the +/- maximum amplitude that the accelerometer can measure before distorting or clipping the output signal. Typically specified in g's.

Frequency Response is determined by the mass, the piezoelectric properties of the crystal, and the resonance frequency of the case. It is the frequency range where the output of the accelerometer is within a specified deviation, typically +/- 5%. g 1g is the acceleration due to the earth's gravity which is 32.2 ft/sec2, 386 in/sec2 or 9.8 m/sec2.

Grounding - There are two types of signal grounding in accelerometers. Case Grounded accelerometers have the low side of the signal connected to their case. As the case is part of the signal path and may be attached to a conductive material, care must be used when using this type of accelerometer to avoid noise from the ground plain. Ground Isolated accelerometers have the electrical components isolated from the case and are much less susceptible to ground induced noise.

High Frequency Limit is the frequency where the output exceeds the stated output deviation. It is typically governed by the mechanical resonance of the accelerometer.

Low Frequency Cut-off is the frequency where the output starts to fall off below the stated accuracy. The output does not "cut-off " but the sensitivity decreases rapidly with lower frequencies.

Noise - Electronic noise is generated by the amplifying circuit. Noise can be specified either broad band (specified over the a frequency spectrum) or spectral - designated at specific frequencies. Noise levels are specified in g's, i.e. 0.0025 g 2-25,000 Hz. Noise typically decreases as frequency increases so noise at low frequencies is more of a problem than at high frequencies.

How to choose an accelerometer?


1. What is the vibration amplitude to be monitored?

2. What is the frequency range to be monitored?

3. What is the temperature range of the installation?

4. What is the size and shape of the sample to be monitored?

5. Are there electromagnetic fields?

6. Is there a high level of electrical noise in the area?

7. Is the surface where the accelerometer is to be mounted grounded?

8. Is the environment corrosive?

9. Does the area require Intrinsically safe or explosion proof instruments?

10. Is the area a wet or a wash down area?

Resonance Frequency is the frequency at which the sensor resonates or rings. Frequency measurements want to be well below the resonance frequency of the accelerometer.

Sensitivity is the output voltage produced by a certain force measured in g's. Accelerometers typically fall into two categories - producing either 10 mV/g or 100 mV/g. The frequency of the AC output voltage will match the frequency of the vibrations. The output level will be proportional to the amplitude of the vibrations. Low output accelerometers are used to measure high vibrational levels while high output accelerometers are used to measure low level vibrations.

Temperature Sensitivity is the voltage output per degree of measured temperature. The sensors are temperature compensated to keep the change in output to within the specified limits for a change in temperature.

Temperature Range is limited by the electronic micro circuit that converts the charge to a low impedance output. Typically the range is -50 to 120C.

Other Considerations when choosing an Accelerometer:

The mass of the accelerometers should be significantly smaller than the mass of the system to be monitored. The accelerometer dynamic range should be broader than the expected vibration amplitude range of the sample. The frequency range of the accelerometer should fit the expected frequency range. The Sensitivity of the accelerometer should produce an electrical output compatible with existing instrumentation. Use a low sensitivity accelerometer to measure high amplitude vibrations and conversely use a high sensitivity accelerometer to measure low amplitude vibrations.

Choose the right accelerometer

Top
Premium Grade Accelerometer Premium Grade Accelerometer
These accelerometers are made from premium selected crystals and use low noise circuitry to product a premium, low noise, accelerometer. Their 316L Stainless steel case is hermetically sealed against the environment so they can survive harsh industrial environments. They also have FM and CSA Intrinsically safe options available. The ACC793 is a standard top cable configuration and the ACC797 is a low-profile side cable configuration.
Industrial Grade Accelerometer Industrial Grade Accelerometer
Industrial grade accelerometers are the workhorses of industry. The are used on everything from machine tools to paint shakers. OMEGA has four models to choose from. ACC101 (shown) is a high quality low cost accelerometer for general purpose applications. ACC 102A is hermetically sealed for harsh environments, has a fixed cable and weighs only 50 grams. The ACC786A, top cable, and ACC787A, side cable, are hermetically sealed and have detachable cables sealed against the weather.
High Vibration Accelerometer High Vibration Accelerometer
Accelerometers used to monitor high vibration levels have a lower output (10 mV/g) and lower mass than industrial accelerometers. The ACC103 weighs 15 gms and can monitor vibration levels up to 500 g's. It is a stud mount design and is designed for use on shaker tables, vibration labs and heavy industrial machine tools. The ACC104 weighs only 1.5 gms and is designed for adhesive mounting. Both models have a Frequency range of 3 to 10 kHz and a dynamic range of +/- 500 g's.
Triaxial Accelerometer Triaxial Accelerometer
Triaxial accelerometers measure the vibration in three axes X, Y and Z. They have three crystals positioned so that each one reacts to vibration in a different axis. The output has three signals, each representing the vibration for one of the three axes. The ACC301 has lightweight titanium construction and 10 mV/g output with a dynamic range of +/-500 g's over a range of 3 to 10 kHz.

Frequently Asked Questions

Top

Mounting an Accelerometer

The sensor must be mounted directly to the machine surface to correctly measure the vibrations. This can be accomplished by several types of mounts:

- Flat Magnet Mount
- 2-pole Magnet Mount
- Adhesives (Epoxy/Cyanoacrylate)
- Mounting Stud
- Isolating Stud

Magnet Mounts are generally temporary mountings.
Magnetic mounts are used to mount accelerometers to ferromagnetic materials commonly found in machine tools, structures and motors. They allow the sensor to be easily relocated from site to site for multiple location readings. Two-pole magnetic mounts are used to mount an accelerometer to a curved ferromagnetic surface.

Adhesives, and threaded studs are considered permanent mountings.
Adhesives such as epoxy or cyanoacrylate have proven to provide satisfactory bonding for most applications. Keep the film as thin as possible to avoid any unwanted dampening of the vibrations due to the flexibility of the film. To remove an adhesive mounted accelerometer, use a wrench on the case's wrench flats and twist to break the adhesive bond. DO NOT USE A HAMMER. Striking the accelerometer will damage it.

Mounting studs are the preferred mounting technique.
They require the structure to be drilled and tapped but provide solid reliable mountings. Be sure to follow the specified torque settings to avoid damaging the sensor or stripping the threads.

Shop for Accelerometers in Australia

The OMEGA Engineering Singapore office handles all inquiries and orders for Australia. We have Application Engineers and Sale Support Staff ready to assist you with your technical questions, quotations and orders. A one-stop source for process measurement and control, OMEGA provides support through web chat, e-mail and telephone. View our contact page to call or email us.